You are here: Tools > AKD into KAS > Workbench User Guide > Controlled Stop (Active Disable)

Controlled Stop

In a controlled stop, drive motion is brought to a standstill in a controlled manner. The drive commands a zero velocity from the motor. The motor decelerates at the prescribed deceleration value (CS.DEC on pg. 1).

A controlled stop can occur in three ways:

The controlled stop mechanism is activated in the following cases:

  1. DRV.DISMODE = 2 and user executes DRV.DIS from the terminal or WorkBench disable buttons.
  1. DRV.DISMODE = 2 and user executes DRV.DIS from a fieldbus connected to the drive.
  2. A fault happens for which the reaction evolves controlled stop (CS). After the CS is executed, the drive disables.
  3. A digital input mode (DINx.MODE) is set to 13. If the digital input state changes (active high or low according to DINx.INV) the CS is executed, and then the drive disables.
  4. HW limit switch: A digital input is defined as a positive (negative) limit switch (DINx.MODE 18 or 19). When the limit switch is met, the CS mechanism starts running. In this case, the parameter DRV.DISTO is not active.
  5. SW limit switch: SWLS defines an active SW limit. When the limit is met, the CS mechanism starts running. In this case, the parameter DRV.DISTO is not active.

Use the drive CS parameters to configure a controlled stop as follows:

  1. CS.DEC: Deceleration ramp that is used for disable.
  2. CS.VTHRESH: Velocity 0 threshold. The motor shaft is considered as stopped as soon as the actual velocity (filtered through a 10 Hz filter, such as VL.FBFILTER) is within ± CS.VTHRESH.
  3. CS.TO: Velocity 0 time. The actual velocity must be consecutively within 0 ± CS.VTHRESH for the time CS.TO, before the drive completes the CS process. This value is used since the motor can overshoot out of the VEL0 window depending on the gains, deceleration ramp, motor inertia and so on.
  4. DRV.DISTO: DisableRemoval of the ENABLE signal. Disables power stage. time out. This parameter sets an overall and independent running check as to whether or not the drive can achieve the disable state. If the VEL0 window set in step 3 is too small, it is possible that the drive may never reach the end of the CS process. The DRV.DISTO parameter and functionality addresses this issue by disabling the drive after the DRV.DISTO time elapses, even if the CS process did not end.

Controlled Stop Diagram

When configuring the controlled stop feature, please note the following:

The drive issues a fault FF703 on pg. 1 in case that the DRV.DISTO counter expires during a controlled stop procedure.

Related Parameters and Commands

CS Parameters on pg. 1

CS.STATE on pg. 1: Reads the current state of controlled stop process (0 = controlled stop is not occurring. 1 = controlled stop is occurring).

DIN1.MODE TO DIN7.MODE on pg. 1

DRV.DIS on pg. 1

DRV.DISTO on pg. 1

DRV.DISMODE on pg. 1

Related topics:

Emergency Stop on pg. 1

Digital Inputs and Outputs on pg. 1

Fault and Warning Messages on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™